About option "No Embed Check" of "Embedded surfaces: G-SU-EM"

2024-01-24T04:11:00Z

Summary


Details

When using the Check-Mate test "Embedded surfaces: G-SU-EM" with the option "No Embed Check" to check for embedded surfaces, do not get correct results.

Though there are embedded surfaces, the check mate test result does not fail and it pass.

Solution

The option “No Embed Check” means that the checker does not validate whether two surfaces are partially overlapped or embedded instead it checks if surfaces are identical to each other. In the case, both surfaces are trimmed B-surface, but they are not identical. You can use the command Information-> B-surface to verify if the surfaces are partially overlapped or embedded to each other.

KB Article ID# PL8768671

Contents

SummaryDetails

Associated Components