SESE resets changes on custom property when performing an additional action

2024-03-21T17:33:24Z

Summary


Details

When a Teamcenter managed assembly and individual components are revised in Solid Edge Structure Editor (SESE), custom properties may also occasionally change.

If in SESE an addition item is set to an action, the previous property changes will be reset to the original value.

Steps To Reproduce:

1. Revise components

2. Change custom properties

3. Set another component to Revise -> the change in step 2 is cleared

Solution

Check if the custom property exists in both SESE grids (left and right sides of screen).  Currently, behavior is that custom properties are cleared in the right hand screen when they are not set to visual in the left hand screen. 

This is by design.

KB Article ID# PL8768498

Contents

SummaryDetails

Associated Components