How to remove the Title Block definition from all tables of the Title Block
SolutionOnce the Title Block has been defined, the Title Block functionality requires atleast one table to be defined.
Since it is the goal to remove all tables from his title block definition, create a dummy table first.
1. Select the 'Tabular Note' icon and place the "dummy" Tabular Note anywhere on the drawing.
2. Hover the cursor over the Title Block, 'MB3-->Edit Definition'.
3. In the Define Title Block dialog, highlight the "Select Tables" prompt.
4. Hold the SHIFT key down and select all the tables in the Title Block to remove those tables from selection.
5. Since the Title Block needs atleast one table, select the "dummy" Tabular Note.
6. OK to finish the command.
7. Delete the "dummy" Title Block table.
Now the tables that were in the Title Block can be edited again as tables.
When the tables are finished with editing, the Title Block will have to be defined again using the 'Define Title Block' command.
Notes