How to change or remove the default connector path?

2024-01-17T12:10:21Z

Summary


Details

A customer wants to know how they can change or remove the default connector path inside Solid Edge. If the customer has a SaaS license, they get the Teamcenter Share feature in their license.  With that feature, they can use Teamcenter Share inside Solid Edge. The connector will automatically set the default path in Solid Edge to the Connector_1 location where the folders "Home" and "Projects" are.

However, the customer finds it inconvenient that it keeps going to that location when saving a file, because most of the time, the customer wants to save the file in the last used location or the location of the original file (home button workaround).  Consequently, they have to change the location each time they want to save a file.

Platforms
  • all n/a-n/a
Release Versions
  • Solid Edge V224UPD2
Solution

Here is how to resolve:

1) Log out

2) Use off-line mode

3) Use SEDM and add another vault

Notes

KB Article ID# PL8767709

Contents

SummaryDetails

Associated Components