Solid Edge Solid Edge 2024 Update 2 Announcement

2024-01-02T17:53:23Z
SE_BETA SE_TSS DOC_MANAGEMENT FLOEFD 3D-SKETCH SIMULATION Teamcenter Share TECH_PUB ASSEMBLY APPLICATION PART/SHEETMETAL TRANSLATORS DRAFT SETUP Solid Edge Marketing

Summary


Details

January 2, 2024

Dear Solid Edge Customer:

Solid Edge 2024 Update 2 is now available for download.

We appreciate your continued business and participation in the software support process. Your feedback helps us improve Solid Edge to better serve your business needs.

Sincerely,

The Solid Edge Team

============

Release Notes:

============

Solid Edge 2024 Update 2

Version: 224.00.02.04

Download Solid Edge 2024 (2310) Updates

Note: if the direct download URL doesn't resolve in your browser, please navigate from the top-level Support Center.

===============

Email Notification:

===============

To receive direct email notifications for Solid Edge Updates, navigate to your Support Center Profile (https://account.sw.siemens.com/profile, scroll to Newsletter Subscriptions, and check the box for Software Field Bulletin

==========================================

This Solid Edge Update resolves the following PRs:

==========================================

===Assembly===

PR 10860687: Design Configurator crashing when picking a part that has an associated draft file

PR 10869082: Show Only not working correctly with a suppressed occurrence selected

PR 10862929: Trim/Extend of Frame taking a long time

PR 10881246: Solid Edge crashes in assembly when you save a movie in the animation editor

PR 8693094: Crash with the Route command when selecting circular edges

===Draft===

PR 10896922:  Breakout on hole causes a crash

===Part/Profile/Sheetmetal===

PR 10808630: Solid Edge crashes with 'Align' and then 'Delete Mesh'

PR 10852686: Feature in FOP members fails for SE2023 while works ok in ST9

PR 10876139: Solid Edge crashes when redefining the diameter of a Hole

PR 10810620: Crash on 'Curve by Table-Edit Points Step'.

PR 10820979: Undo command memory is cleared when interpart links are frozen

PR 10893147: Ultra unlock encountered an error when running the standard nesting engine

===Solid Edge Data Management===

PR 8695881: Where used and Open Drawing not working as expected in non-auto number set up

===Translators===

PR 10838049: Material transfer from Solid Edge to NX is not working as expected

PR 10879634: Inventor migration fails

PR 10813723: The thread pitch defined in Solid Edge parts is not properly transferred to CAM Pro

PR 12000665: Digits after delimiter are not taken out when exporting an STL file

KB Article ID# PL8766680

Contents

SummaryDetails

Associated Components

SE_BETA