Uninstalling Solid Edge 2023 without also uninstalling Solid Edge 2023 Design Configurator will block the installation of Solid Edge 2024 -- Error: Setup has detected that another Solid Edge product is currently installed. The existing product must be uninstalled for setup to continue.
The error message does not indicate that the 2023 Design Configurator is blocking the installation of Solid Edge 2024.
Further confusion is caused due to Design Configurator not being listed in Add/Remove Programs the same as other Solid Edge products, so it is unclear to the user that the Solid Edge 2023 Design Configurator is still installed and is blocking the installation of Solid Edge 2024.
SolutionUninstall "Design Configurator for Solid Edge 2023"