How to create a JT with an assembly as a single file i.e., MONOLITHIC in manage mode in NX using the save option "Save JT Data".

2023-12-29T10:21:35Z

Summary


Details

How to create a JT with an assembly as a single file i.e., MONOLITHIC in manage mode in NX using the save option "Save JT Data".

*The following settings in the configuration file

structureOption = "MONOLITHIC"

writeWhichFiles = "JTPARTS,JTASSEMBLY"

When exporting JT from NX to OS, we can export the assembly as a single file. However, we cannot create a JT on Teamcenter with the same settings. (Use the save option "Save JT Data").

Solution

With GUI it's not possible in Manage mode, you must use the command line utility only.

The run_ugtopv command was able to create a monolithic JT in manage mode.

In the NX {UGII_BASE_DIR}\PVTRANS directory there is a default tessUG.config.

Inside "your_tess.config" file change:

structureOption = "PER_PART"

to

structureOption = "MONOLITHIC"

Use the below sample syntax for the JT Translation.

{UGII_BASE_DIR}\PVTRANS\run_ugtopv @DB/itemID/Item_REV -pim=yes -u=user

-p=password -g=group -honour_structure

(Replace {UGII_BASE_DIR} with the full path for the command line.

KB Article ID# PL8766114

Contents

SummaryDetails

Associated Components