NX About the "Naming Tab" in the Export Assembly from Teamcenter dialog with the latest NX release.

2023-12-29T10:20:52Z
NX for Design

Summary


Details

About the "Naming Tab" in the Export Assembly from Teamcenter dialog with the latest NX release.

In NX11, select Export Name: User Number from the Naming Tab of Export Assembly Dialog. We were able to use it, but the User Number is missing in the latest NX release like NX2306. How do we get these options?


Solution

Users can select the Auto Translate option with the latest NX release and manually type in by editing the cell value. Earlier it used to launch another dialog to get the user input, with the new user interface it is not required.


KB Article ID# PL8766112

Contents

SummaryDetails

Associated Components

Teamcenter Integration for NX