Solid Edge 2023 Update 0010 Announcement

2023-12-14T21:51:54Z

Summary


Details

December 14, 2023

Dear Solid Edge Customer:

Solid Edge 2023 Update 0010 is now available for download.

We appreciate your continued business and participation in the software support process. Your feedback helps us improve Solid Edge to serve your business needs better.

Sincerely,

The Solid Edge Team

============

Release Notes:

============

Solid Edge 2023 Update 0010

Version: 2210.0009.003 x64

Download Solid Edge 2023 (2210) Updates

Note: if the direct download URL doesn't resolve in your browser, please navigate from the top-level Support Center.

===============

Email Notification:

===============

To receive direct email notifications for Solid Edge Updates, navigate to your Support Center Profile (https://account.sw.siemens.com/profile, scroll to Newsletter Subscriptions, and check the box for Software Field Bulletin

==========================================

This Solid Edge Update resolves the following PRs:

==========================================

===Assembly===

PR 10465633: Tube part update changes item number

PR 10803960: Associate with Material switch Bend Radius to Value of another Material

PR 10845733: PMI dimensions disappearing while being repositioned

PR 10858970: Issues with new assembly features - relevant changes to backport for WIPRO

PR 10858989: Issues with Peer Edge locate/highlight after changing plane on a profile-based feature

PR 10859226: Updates made to a Part file are not reflected in all ASM features that use that part

PR 10867386: PathFinder content disappears while selecting components if 'Auto-scroll assembly

PR 10869082: Show Only not working correctly with a suppressed occurrence selected

PR 10862929: Trim/Extend of Frame taking a long time

PR 8693094:  Crash with the Route command when selecting circular edges

===Draft===

PR 10783004: Area Moments change significantly based on distance from the file origin

PR 10820498: Wrong Dimension values displaying in Draft file with Broken View

PR 10857577: Break Line Pair selected via left-click cannot be deleted with the Delete key

PR 10858562: Solid Edge API cannot set a PartList cell value

===Part/Profile/Sheetmetal===

PR 10374475: Problems using "Undo" in a sketch of an in-place activated file of an assembly

PR 10717733: Hole Tolerance Class is incorrect in Hole Callout.

PR 10851422: Round command radius value resets to .125" when accept clicked

PR 10861021: Crash when choosing Cancel in the error dialog of Bend Bulge Relief

PR 10861144: Crash when the settings of a Fillet Weld is selected

PR 10862197: Crash while using a sketch in the part environment

PR 10863599: SE2023 up9 crashes when editing the sketch

PR 10808630: Crash when choosing 'Align' then 'Delete Mesh.'

PR 10810620: Crash on 'Curve by Table-Edit Points Step'

PR 10820979: Undo command memory is cleared when interpart links are frozen

PR 10852686: Feature in FOP members fail

PR 10876139: Crash when redefining the diameter of a Hole

===SEEC===

PR 10778454: Opening an assembly from structure manager opens the wrong part

PR 10789095: Some files are failing to index into Geolus

===Data Management===

PR 8695881: Where used and Open Drawing not working as expected in non-auto number set up

===Translators===

PR 10781221: Save As DWG is slow if the seacad.ini options file is on a file share

PR 10820922: Inventor constraints are not migrated to Solid Edge relationships

PR 10821215: After opening dwg and dxf files, Solid Edge crashes

PR 10839334: Inventor data migration aborts after 35 translated files

PR 10858323: Import IFC file results in a crash

PR 10879634: Inventor migration fails ( invalid pointer )

PR 8669242: Import of IFC files cannot be opened or are faulty

KB Article ID# PL8764840

Contents

SummaryDetails

Associated Components