Why have I received a 'cdlmd' license file containing 'DOEtoken' features?

2024-09-13T09:34:32Z

Summary


Details

In addition to the NX (ugslmd) license file, a separate 'cdlmd' license (containing 'DOEtoken' features) was supplied.

What is this license for and how should be deployed?

Solution

If you have any of the following NX product in your configuration:

NX13110 / NX93110 - NX MACH 3 Additive Design with Convergent

NX30710 - NX Advanced Convergent Modeling Add-on

NXS30110 - NX Additive Design with Convergent Sticky Add-on

You will receive an additional 'Simcenter STAR-CCM+' (cdlmd) license file, containing 10 'DOEtoken' features for each of the products listed above.

The NX Polygon Modelling functionality includes two commands ('Wrap Mesh' and 'Plug Leakage') that are implemented using STAR-CCM+ functionality.

NX Polygon Modeling - 'Wrap Mesh' & 'Plug Leakage' commands

To enable these two particular commands, an installation of Simcenter STAR-CCM+ is required as well as the 'cdlmd' license file containing the 'DOEtoken' features.

For further information, on how to install and license Simcenter STAR-CCM+ for this purpose, please refer to the following article on the Support Center: Simcenter STAR-CCM+ Installation Process for NX 'Wrap Mesh' and 'Plug Leakage' commands, using the Siemens License Server (SLS v2.1) 

Notes

KB Article ID# PL8763657

Contents

SummaryDetails

Associated Components