Solid Edge Add to Teamcenter Interactive - Only one Solid Edge Document...

2024-08-28T12:45:30Z
DOC_MANAGEMENT

Summary


Details

While using Add to Teamcenter Interactive an error is occurring, "There can only be one Solid Edge file document per revision".

Platforms
  • na windows-1064
Release Versions
  • Solid Edge V222MP14
Solution

Check to see if there are multiple Solid Edge datasets in Teamcenter that use the same name. How this occurs is unknown. Use unique names to resolve the issue.

Notes

KB Article ID# PL8763540

Contents

SummaryDetails

Associated Components

DOC_MANAGEMENT: SEEC