2D Nesting - "Ultra unlock encountered an error, running standard nesting engine"

2023-12-22T13:28:32Z

Summary


Details

The user is getting the following error message when using Solid Edge 2D Nesting:


Steps To Reproduce: 

-Start 2D Nesting

-Select "import parts" dxf/dwg button, select a *.dxf files

-Select sheet tab and create sheet, select a sheet or create a sheet if non available.

-Select nesting tab, click the start button.

Problem: Error "Ultra unlock encountered an error, running standard nesting engine" pops up.

The problem is that without this function is that it will not rotate the component for best fit.

Platforms
  • na windows-1064
Release Versions
  • Solid Edge V224UPD1
Solution

This is a particularly rare issue - the fix will be supplied in an update to the application Solid Edge 2D Nesting.

Notes

KB Article ID# PL8763528

Contents

SummaryDetails

Associated Components