- In NXManager, after executing
File --> Export --> STEP
nxmgr shows an unexpected default dataset name.
- The Export STEP File dialog,
after setting Output File Destination to
Teamcenter
shows "MFK" as part of the dataset name value
- However, MFK ( MultiFieldKey ) has not been implemented
for use with these nx/manager part types.
- Also occurs with default OOTB type of Item.
Solution- The preference
TC_MFK_DEFAULT_DOMAIN
did not have a value.
- After setting to the default value of
Item
the default Dataset Name value
included item id and revision id
*without* "MFK"
Also occurred with Export IGES File dialog window.