PMI report command does not exist

2023-12-01T01:00:15Z

Summary


Details

The following documentation describes how to access the PMI report command, but I cannot find it in the location specified as "Menu".

https://docs.sw.siemens.com/en-US/doc/209349590/PL20220512394070742.pmi/pmi_general_info_pmi_report


Reproduced Steps:

1. Open new part and go to PMI environment

2. Menu > Information > PMI > Report

** PMI Report does not exist.


Reference: NX 2206 and lower can find the command.


Solution

This is because the documentation has not been updated even though PMI Report command is now treated as a legacy command in NX 2212 Series.

PMI Report, PMI Search, and Find PMI Associated to Geometry content are moved to the "Legacy" section of NX 2312 documentation, and add a note indicating that the functionality is replaced with MBD Query command.

Notes

 - MBD Query command(Menu > Information > Query)

Documentation :

https://docs.sw.siemens.com/ja-JP/doc/209349590/PL20220512394070742.mbd/xid1978452

 - Legacy PMI Report command can be accessed from "Customize...".(Ctrl+1).

**Please refer to PL8762222 for Japanese article.

Release Versions
  • NX V2212
  • NX - PMI V2212
Platforms
  • Windows x64 10
  • Windows x64 11

KB Article ID# PL8762224

Contents

SummaryDetails

Associated Components