NX crashes unexpectedly when repeating dimension alignment operations

2023-12-01T00:57:15Z

Summary


Details

NX crashes when repeatedly performing mouse drag operations to align dimension line placement positions.

Reproduced Steps:

1. Align to a certain dimension

2. Perform the operation to align one of the aligned dimensions to the left or right dimensions again.

3. Repeat the operation using another dimension

**If you repeat the same operation to change the related parent like this, NX will crash unexpectedly.

Solution

This issue is due to NX problem and happened NX 1953 Series and lower, but has been fixed in NX 1980 Series.

Workaround : In case of Mouse Dragging operation there is no effective way. Please use Origin Tool ( select a dimension > Mouse right click > Origin > each Alignment tool)


Notes

The problem occurs with all dimension types, not just linear dimensions, but ordinate dimensions.

**Please refer to PL8762219 for Japanese article.

Release Versions
  • NX V1926
  • NX - DRAFTING V1926
Platforms
  • Windows x64 10
  • Windows x64 11

KB Article ID# PL8762220

Contents

SummaryDetails

Associated Components