In this scenario, the user has a Solid Edge assembly. While checking the Assembly Features, they notice that the position of the hole does not correspond to that defined within the sketch profile.
The distance dimension of the hole created as an assembly feature shows 55 mm.
However, when editing the sketch of the assembly feature, the distance is different - 40 mm.
The assembly document believes it is up to date with the part having been modified by the hole, and since it thinks it is, it will not update until the body in the part document is considered modified.
The workaround is to select and edit the part, modify the body (example: change the 160 dimension to 155 and then back to 160), close and return to the assembly - this will force the assembly feature to update.
The dimension that previously indicated 55 mm is now correctly showing 40 mm.