Default program doesn't run the desired operations, other operations run instead.

2024-01-18T21:06:09Z

Summary


Details

Default program doesn't run the desired operations, other operations run instead.

Platforms
  • na windows-1064
Release Versions
  • Tecnomatix V_UNKNOWN
Solution

When you have multiple programs in Line Simulation, you have to block all operations as PS lets multiple operations to run in parallel.

So you need to:

- group your operations (per program) each under a compound operation.

- add an operation named "BLOCK" (name can be anything, "BLOCK" just for explanation purposes) prior to your set of grouped operations.


- Make its transition value to FALSE

- Connect BLOCK to your grouped operations (in the sequence editor). Then the default main program will handle which operations should run.


Notes

KB Article ID# PL8760657

Contents

SummaryDetails

Associated Components