Can the Solid Edge file property "Project Name" be mapped to a Teamcenter attribute?

2023-11-20T18:36:51Z

Summary


Details

Can the Solid Edge file property "Project Name" be mapped to a Teamcenter attribute?

Platforms
  • na windows-1032
Release Versions
  • Solid Edge V221.0
Solution

Project Name is a reserved Solid Edge file property that is already in use.

When creating custom mapping, do not use the following Solid Edge properties:

Teamcenter Item Type

Document Number

Revision Number

Project Name

Dataset Name

TC Engineering DescriptionThose properties are in use as defined in the SEEC administrator's guide.

Notes

KB Article ID# PL8760430

Contents

SummaryDetails

Associated Components