Solid Edge Classic Plus licenses cannot be checked out from the license server

2024-08-05T04:10:14Z

Summary


Details

The customer has a Solid Edge Mechanical Design bundle which contains multiple Solid Edge Classic Plus licenses which they cannot check out from the license server.  The customer uses Solid Edge 2020.

Platforms
  • all n/a-n/a
Release Versions
  • Solid Edge V220MP14
Solution

The reason for this is that Solid Edge Mechanical Design Bundle was introduced for Solid Edge 2021 and is only supported by Solid Edge 2021 MP1 and later versions.

Notes

If you have further inquiries about floating Licensing please refer to the FAQs collection link below:

Solid Edge Floating License FAQs Collection


KB Article ID# PL8760042

Contents

SummaryDetails

Associated Components