Solid Edge Error when opening Standard Parts Administrator 2023

2023-11-27T16:08:08Z
APPLICATION

Summary


Details

In this scenario, the installation of Solid Edge 2023 including Standard Parts happened without error messages, but the user subsequently receives an error regarding Microsoft .NET Framework on opening of the Standard Parts Administrator (PMAdministrator.exe).

Solution

This is possibly because they did not install Update 1 before the installation of the Standard Parts Administrator.

This can be corrected as follows:

- Uninstall Standard Parts Administrator

- Restart the system

- Install Update 1

- Install .NET Framework 4.8 from the Solid Edge 2023 installation software in 

  ...\Solid Edge\ISSetupPrerequisites\DotNET4.8

- Install Standard Parts Administrator

- Install the latest Update

- Restart the system

Notes

The need to install Update 1 or any later update before the installation of the Standard Parts Administrator (StandardPartsAdministrator_2023_2210_[language].exe) is an exception in Version 2023.  Nevertheless, it is imperative to also install the latest update after the installation of the Administrator software.  Solid Edge software updates often include fixes for Standard Parts software.

KB Article ID# PL8759189

Contents

SummaryDetails

Associated Components

APPLICATION: STANDARD_PARTS