Solid Edge Recommended versions of Windows 11 for SE2024

2024-02-19T16:50:04Z
APPLICATION SETUP

Summary


Details

What are the current recommended versions of Windows 11 for Solid Edge 2024?

Solution

All versions of Windows 11 (Professional and higher editions) that are currently in the active servicing timeline provided by Microsoft (https://learn.microsoft.com/en-us/windows/release-health/windows11-release-information) are supported with Solid Edge 2024.

Our recommendation has always been that customers should delay taking Windows Feature Updates (new versions/operating systems) for as long as possible (https://support.sw.siemens.com/knowledge-base/PL8008188). This is because we believe that maturer Windows versions provide for more overall stability than newer recently released Windows 11 versions.

As the maturest Windows 11 version approaches end of servicing with Microsoft we would then recommend that customers begin migrating over to the next maturest Windows 11 version that is actively supported by Microsoft.

As such, at this time, we recommend that customers should be using Windows 11 version 22H2 as it is the most mature actively supported version of Windows 11. As 22H2 approaches end of servicing with Microsoft we would then recommend customers begin migrating over to the next maturest supported version of Windows 11 which is currently version 23H2.

KB Article ID# PL8758452

Contents

SummaryDetails

Associated Components

APPLICATION: OTHER