Shake gesture removes sketch dimensions

2023-11-07T01:24:53Z

Summary


Details

When a sketch shape is moved using Shake Gesture, its attached dimensions are removed.

Reproduced Steps:

1. Create sketch shapes and a dimension


2. Move the dimension with Shake Gesture

***When the move operation is completed, the attached dimensions will be removed.


Solution

This behavior is working as designed.

Workaround : Use Ignore Relation or Relax Dimensions commands as appropriate. (See the NOTES link for instructions on how to use these commands.)

= Ignore Relation =


= Relax Dimensions =


Notes

Ignore Relation :

https://docs.sw.siemens.com/en-US/doc/209349590/PL20221117716122093.xid1849545/xid1849937

Relax Dimensions :

https://docs.sw.siemens.com/en-US/doc/209349590/PL20221117716122093.xid1849545/xid1849841

***Please refer to PL8758176 for Japanese article.

Release Versions
  • NX V2212
  • NX - DESIGN V2212
Platforms
  • Windows x64 10
  • Windows x64 11

KB Article ID# PL8758177

Contents

SummaryDetails

Associated Components