The interference distance detected by interference checking is not displayed as the tag

2023-11-06T04:56:44Z

Summary


Details

When trying to display tags in the graphics window for interference results detected by Clearance Browser, some tags (interference distance) are not displayed.

Reproduced Steps:

1. Prepare assembly parts exists 21 or more interferences

2. Menu > Analysis > Assembly Clearance > Clearance Set > New > OK

3. Display all detected interference results in Clearance Browser using tags (turn on the display/hide toggle)

***You can confirm that only up to 20 tags are displayed.


Solution

This behavior is working as designed.

Workaround : Limit the number of tags to be displayed at one time to 20, and divide the operation into multiple steps.

Notes

We currently have limited functionality because the memory consumption for displaying tags is very large and affects performance. In order to remove the limitation, a large-scale algorithm change is required, and we have received several requests for enhancements.

***Please refer to PL8758173 for Japanese article.

Release Versions
  • NX V2212
  • NX - DESIGN V2212
Platforms
  • Windows x64 10
  • Windows x64 11

KB Article ID# PL8758175

Contents

SummaryDetails

Associated Components