NX tcin_import not loading revisions with same item_id from clone log file

2023-12-30T15:39:22Z
NX for Design

Summary


Details

Error importing two revisions of the same Item


Solution

Ensure the Multiple Revisions is set to ON in the customer defaults.

The command prompt should be set with the correct variable pointing to the customer default setting that has the Multiple Revisions set to ON.

Notes

KB Article ID# PL8756249

Contents

SummaryDetails

Associated Components

Teamcenter Integration for NX