Unable to create spline in drawing view

2023-10-30T03:16:36Z

Summary


Details

When trying to create a sketch spline in a drawing view, it is not created on the view plane but on the orthogonal plane.

Reproduced Step:

1. Create a view (other than Top) in a drawing sheet


2. Select a view boundary > Active Sketch View > go to Sketch tab > Spline


3. Create a spline whenever you want



Solution

This behavior is NX bug that only occurs in NX 2306 Series and will be fixed in NX 2312 Series.

Workaround : Create a sketch shape other than a spline ( such as line, circle or etc.) in advance and create a spline. Then, delete the unnecessary sketch shapes created in advance.

Notes

This behavior occurs when the coordinate system of the drawing view is other than XY plane (Top view).

***Please refer to PL8756220 for Japanese article.

Release Versions
  • NX V2306
  • NX - DESIGN V2306
Platforms
  • Windows x64 10
  • Windows x64 11

KB Article ID# PL8756221

Contents

SummaryDetails

Associated Components