Differences between two types of drawing template parts provided by Siemens

2023-10-30T03:16:14Z

Summary


Details

There are two types of template parts for each size in the NX installation folder (example: ~NX2212\DRAFTING\templates). I opened them up and looked at their contents, and they look the same. Is there any difference?


Reproduced Steps:

1. Open “Drawing-A4-Size-template.prt” and “Drawing-A-Size2D-template.prt” and compare them.

Solution

The two types of template parts Siemens provides has the same content, but are used differently depending on NX command used.

“Drawing-A4-Size-template.prt”

  -  Used when "Reference Existing Part" is selected when creating a new drawing (File > New > Drawing tab)   **(1)

“Drawing-A-Size2D-template.prt”

  -  Used when "Stand-alone Part" is selected when creating a new drawing (File > New > Drawing tab)   **(2)

  -  Used when creating a new sheet with New Sheet command   **(3)

Notes

"ugs_drawing_templates.pax" specifies the template part that will be used when **(1) and (2) are executed. "ugs_sheet_templates.pax" specifies the template part that will be used when **(3) is executed.



Documentation for Drawing Templates :

https://docs.sw.siemens.com/en-US/doc/209349590/PL20220512394070742.drafting/xid1107611

***Please refer to PL8756028 for Japanese article.

Release Versions
  • NX V2212
  • NX - DRAFTING V2212
Platforms
  • Windows x64 10
  • Windows x64 11

KB Article ID# PL8756030

Contents

SummaryDetails

Associated Components