Component that is not cut by PMI Section View is displayed in a cut state after exporting Technical Data Package

2023-10-25T00:40:27Z

Summary


Details

There is a component in the assembly that is cut by PMI Section and a component that is not cut by PMI Section. In this state, if performing 3D PDF export using Technical Data Package and view it with PDF reader, the component to which PMI cross section has not been applied will also be displayed in the cut state.

Reproduced Steps:

1. Menu > PMI > Section View > OK

  Create a PMI Section View by targeting one component


2. File > Export > Publish Technical Data Package > OK

  Method = 3D PDF


3. Open the exported PDF in a reader such as Acrobat Reader


Solution

This behavior is working as designed.

In addition, in NX 2312 series, the function is enhanced so that only components to which PMI Section View is applied is exported in the cut state.

Workaround: There is no effective workaround.

Notes

****Please refer to PL8755461 for Japanese article.

KB Article ID# PL8755464

Contents

SummaryDetails

Associated Components