Vertical text entered in a Tabular Note extends beyond the frame of the cell row

2023-10-25T00:39:07Z

Summary


Details

If entering a vertical text in a Tabular Note, it will extend beyond the cell row frame. Is it possible to enter without it sticking out?

Reproduced Steps:

1. “Customer Default > Drafting > General/Setup > Standard > Customize Standard > Table > Common > Cell (tab)” and check “Vertical Text” ON > OK


2. Restart NX and open a new part

3. Insert a Tabular Note in Drafting( make sure to set “Auto Size Row” as “Fit Method” for the cell)


4. double-click a cell and input a test( ex,. “1234567890”)



Solution

The behavior is working as designed.

In addition, in NX 2312 series, the function is enhanced so that it does not extend beyond the cell row frame.

Workaround: Please change the cell row size manually.

Notes

***Please refer to PL8755458 for Japanese article.

Release Versions
  • NX V11.0.2
  • NX - DRAFTING V11.0.2
Platforms
  • Windows x64 10
  • Windows x64 11

KB Article ID# PL8755459

Contents

SummaryDetails

Associated Components