Step by Step procedure in implementing the use of PAX files in NX Managed Mode. PAX files are stored in the Teamcenter database.
SolutionStep 1 - Please review the attached video before proceeding.
Step 2 - If the preference does not exist...you must create it. Please see image below...
Step 3 - With the "Definition" tab selected ...be sure the "Name" field = TC_NX_FileNewPAXFiles
Step 4 - The "Category" field is set to "General"
Step 5 - The "Mulitple" field is set to "Multiple"
Step 6 - Add the Item/Rev of the Item that is storing the PAX files.
Step 7 - Create a folder to organize your "pax" files. Please see image below...
Step 8 - Select the folder and create the new "ITEM" for each unique pax file. Please see image below...
Step 9 - Select the "ITEM" revision of each ITEM in order to create the dataset that will hold the individual datasets
Ste 10 - Each dataset will hold "Text". You will import the appropriate pax file into the dataset.