Solid Edge Which FlexLM License Server will work with Solid Edge 2024 ?

2024-08-05T03:45:13Z
SETUP

Summary


Details

In this scenario, a customer finds that the FlexLM License Server delivered with Solid Edge 2023 will not work with Solid Edge 2024.  

When using the FlexLM License Server from Solid Edge 2023, they get the following error message:


Which FlexLM License Server version is needed for Solid Edge 2024 ?

Solution

With Solid Edge 2024 we also provide a new FlexLM License Server version.  This can be found within Support Center > Solid Edge 2024 >Solid Edge 2024 Add-ons:


When unzipping the SptTools_2024_2310.zip, you will see the following:


This License Server is version 2.2.0 which replaces the ugslmd vendor daemon with the new common saltd vendor daemon. 

Notes

If you have further inquiries about floating Licensing please refer to the FAQs collection link below:

Solid Edge Floating License FAQs Collection


KB Article ID# PL8754160

Contents

SummaryDetails

Associated Components

SETUP: LICENSING