Solid Edge Solid Edge 2023 Update 0009 Announcement

2023-10-16T16:24:53Z
SE_BETA SE_TSS DOC_MANAGEMENT FLOEFD 3D-SKETCH SIMULATION Teamcenter Share TECH_PUB ASSEMBLY APPLICATION PART/SHEETMETAL TRANSLATORS DRAFT SETUP Solid Edge Marketing

Summary


Details

October 16, 2023

Dear Solid Edge Customer:

Solid Edge 2023 Update 0009 is now available for download.

We appreciate your continued business and participation in the software support process. Your feedback helps us improve Solid Edge to better serve your business needs.

Sincerely,

The Solid Edge Team

============

Release Notes:

============

Solid Edge 2023 Update 0009

Version: 2210.0009.004 x64

Download Solid Edge 2023 (v2210) Updates

Note: if the direct download URL doesn't resolve in your browser, please navigate from the top-level Support Center.

===============

Email Notification:

===============

To receive direct email notifications for Solid Edge Updates, navigate to your Support Center Profile (https://account.sw.siemens.com/profile, scroll to Newsletter Subscriptions, and check the box for Software Field Bulletin

==========================================

This Solid Edge Update resolves the following PRs:

==========================================

===Assembly===

PR 10491750: Pipe/Frame cut length issues with IAC/Mirror - Create case

PR 10503776: Pipe/Frame cut length issues with IAC/Mirror - Edit case

PR 10746062: Crash when routing a 3D curve

PR 10761767: 'Project Name' not filled with the part name when 'Extending existing part(s)'

PR 10804341: IAC not showing assembly features

PR 10824984: Crash when using a suppressed part with the select identical parts command

PR 10829199: Text display anomaly with Czech L10N during highlight operations

PR 10535394: Frame cut length error

PR 10751446: Solid Edge crashes during Multi-Body Publish

PR 10801921: Revision of Family of assembly has incorrect SE Status Released

PR 10719428: Dimension is causing an Assembly Feature to go warned

PR 10772195: Assembly Feature on a frame not updating when Frame is updated

PR 10844992: Edits to IAC not showing up on screen

PR 10830967: Interpart links are not showing up

===Draft===

PR 10835801: Unblock command in Draft is causing Solid Edge to crash

===Part/Profile/Sheetmetal===

PR 10816588: Solid Edge freezing up in Hole Options dialog on Windows 11

PR 10837889: Crash in Solid Edge when editing a sketch

===SEEC===

PR 10813039: Performance degradation opening assembly after TC 13.3 upgrade

PR 10487459: Error checking in an assembly with adjustable internal component subassembly

PR 10821993: Open draft will modify ASM structure unattended

PR 10739703: The BOM line is not found during an upload

===Tech Pub===

PR 10791751: Errors on Technical Publications HTML export

PR 10835790: Not able to reopen after creating a new file

KB Article ID# PL8754098

Contents

SummaryDetails

Associated Components

SE_BETA