How to export and import kinematics from NX into Process Simulate?

2024-08-26T15:38:32Z

Summary


Details

How to export and import kinematics from NX into Process Simulate?

Platforms
  • na windows-1032
Release Versions
  • Tecnomatix V2206
Solution

The following applications in NX have a command to export the kinematics:

Line Designer -> "Export Kinematics"

Fixture Designer -> "Export Kinematics"

Mechatronics Concept Designer -> "Export plmxml"

To see the commands, you need to load NX from Teamcenter, once used it creates a “kinematics” dataset with a kin.plmxml file in Teamcenter.

Then you can use the Tecnomatix utility ahead to merge the .jt and the kin.plmxml files.  

<install_dir>\Tecnomatix_<version>\eMPower\TxImportKinematicsToJt.exe:

Details on the utility ahead:

PLMXML - based Kinematics Importer

Notes

KB Article ID# PL8753252

Contents

SummaryDetails

Associated Components