Using Delete Machine Code Function

2023-10-10T08:11:44Z

Summary


Details

If the user wishes to post-process an operation or Program Group that has already been posted, an alternative dialog is displayed. This dialog does not allow the user to select a different post-processor. It may be the case in some instances that alterations are not required but the output needs to be produced again. The user will not want to re-generate the operations as this could be time consuming. 

Solution

Using the Machine Code - Delete function allows the original post-process dialog to be displayed and then the user has all capability to select the post-processor they require. This can be a time saving action. This can be achieved by right-clicking (MB3) on the previously posted operation or Program Group and selecting 'Machine Code' -> 'Delete'. 

KB Article ID# PL8752671

Contents

SummaryDetails

Associated Components