After changing PMI Preferences, a font does not change even after performing the reset command

2023-10-12T10:54:02Z

Summary


Details

I changed the font and the height of "Lettering" and "Dimension Text" using "PMI Settings", and performed "Reset All PMI Settings" command. The height was changed, but the font was not changed.

Reproduced Steps:

1. Create PMI Dimension and Note(Font=kanji, Height=3.5)


2. File > PMI > Preferences(e.g., change Font=Arial, Height=10mm)

  -1. Common > Lettering


  -2. Dimension > Text > Dimension Text


3. Menu > PMI > Reset All PMI Settings


4. Confirm the preference of the dimension( select the dimension > Mouth light click > Settings)


Solution

The behavior is working as designed.

Notes

“Reset All PMI Settings” command is the function to resets only the values related to size such as height. Settings such as fonts and arrows are not included.

***Please refer to PL8752587 for Japanese article.

Release Versions
  • NX V2212
  • NX - DESIGN V2212
Platforms
  • Windows x64 10
  • Windows x64 11

KB Article ID# PL8752588

Contents

SummaryDetails

Associated Components