NX Checking out the data in Active Workspace does not show checked out in NX

2023-10-27T12:49:03Z
NX for Design

Summary


Details

Checking-out the ItemRevision in Active Workspace does not show the checked-out status in NX.

Solution

This is because NX does not check-out the ItemRevision. NX will check-out the dataset.

Check-out the dataset in Active Workspace instead to see if the Check-out status appears in NX.

Notes

KB Article ID# PL8752169

Contents

SummaryDetails

Associated Components

Teamcenter Integration for NX