Tecnomatix Controllers for FANUC_RJ, FANUC_RJ_JAPAN, STAUBLI_VAL

2023-10-02T05:50:01Z

Summary


Details

Dear Siemens Digital Industries Software Customer,

We are pleased to inform you that Tecnomatix controllers for "FANUC_RJ, FANUC_RJ_JAPAN, STAUBLI_VAL"

are available for download from https://support.sw.siemens.com.

See Tecnomatix_Controller_Name_changes_log.htm for details concerning this update.

Note: This file is located in the 'OLP Change Logs' folder directly under the 'Process Simulate Robot Controllers' folder.

Use the following steps to download:

- Login to https://support.sw.siemens.com

- If you do not have an account, click 'Register Now' and fill out the information.

- Once on Support Center, if you do not see Tecnomatix under 'My Products', click 'Manage Products'.

- Scroll down and toggle On the Tecnomatix product.

- Scroll back to the top and click Support Center in the breadcrumb.

- Select 'Tecnomatix' from 'My Products'

- Select 'Download'

- Select 'Additional Downloads'

- Select 'Process Simulate Robot Controllers'

- Select 16.0, 16.1, 16.1.1, 16.1.2, 17.0, 2206, 2301 or 2307

[Or Select 'Older Versions' to access 15.1 or 15.1.2]

Download the file(s):

Tecnomatix_15.1_FANUC_RJ_64BIT_v3.90.4_29_09_2023.exe

Tecnomatix_15.1_FANUC_RJ_JAPAN_64BIT_v2.163.4_29_09_2023.exe

Tecnomatix_15.1_STAUBLI_VAL_64BIT_v4.17_29_09_2023.exe

Tecnomatix_15.1.2_FANUC_RJ_64BIT_v3.90.4_29_09_2023.exe

Tecnomatix_15.1.2_FANUC_RJ_JAPAN_64BIT_v2.163.4_29_09_2023.exe

Tecnomatix_15.1.2_STAUBLI_VAL_64BIT_v4.17_29_09_2023.exe

Tecnomatix_16.0_FANUC_RJ_64BIT_v3.90.4_29_09_2023.exe

Tecnomatix_16.0_FANUC_RJ_JAPAN_64BIT_v2.163.4_29_09_2023.exe

Tecnomatix_16.0_STAUBLI_VAL_64BIT_v4.17_29_09_2023.exe

Tecnomatix_16.1_FANUC_RJ_64BIT_v3.90.4_29_09_2023.exe

Tecnomatix_16.1_FANUC_RJ_JAPAN_64BIT_v2.163.4_29_09_2023.exe

Tecnomatix_16.1_STAUBLI_VAL_64BIT_v4.17_29_09_2023.exe

Tecnomatix_16.1.1_FANUC_RJ_64BIT_v3.90.4_29_09_2023.exe

Tecnomatix_16.1.1_FANUC_RJ_JAPAN_64BIT_v2.163.4_29_09_2023.exe

Tecnomatix_16.1.1_STAUBLI_VAL_64BIT_v4.17_29_09_2023.exe

Tecnomatix_16.1.2_FANUC_RJ_64BIT_v3.90.4_29_09_2023.exe

Tecnomatix_16.1.2_FANUC_RJ_JAPAN_64BIT_v2.163.4_29_09_2023.exe

Tecnomatix_16.1.2_STAUBLI_VAL_64BIT_v4.17_29_09_2023.exe

Tecnomatix_17.0_FANUC_RJ_64BIT_v3.90.4_29_09_2023.exe

Tecnomatix_17.0_FANUC_RJ_JAPAN_64BIT_v2.163.4_29_09_2023.exe

Tecnomatix_17.0_STAUBLI_VAL_64BIT_v4.17_29_09_2023.exe

Tecnomatix_2206_FANUC_RJ_64BIT_v3.90.4_29_09_2023.exe

Tecnomatix_2206_FANUC_RJ_JAPAN_64BIT_v2.163.4_29_09_2023.exe

Tecnomatix_2206_STAUBLI_VAL_64BIT_v4.17_29_09_2023.exe

Tecnomatix_2301_FANUC_RJ_64BIT_v3.90.4_29_09_2023.exe

Tecnomatix_2301_FANUC_RJ_JAPAN_64BIT_v2.163.4_29_09_2023.exe

Tecnomatix_2301_STAUBLI_VAL_64BIT_v4.17_29_09_2023.exe

Tecnomatix_2307_FANUC_RJ_64BIT_v3.90.4_29_09_2023.exe

Tecnomatix_2307_FANUC_RJ_JAPAN_64BIT_v2.163.4_29_09_2023.exe

Tecnomatix_2307_STAUBLI_VAL_64BIT_v4.17_29_09_2023.exe

To Install:

Place Tecnomatix_<TecnomatixVersion>_<ControllerName>_NNBIT_vVV_MM_DD_YYYY.exe into a folder ($Tecnomatix/downloads is suggested, where $Tecnomatix is the full path to the Tecnomatix installation).

Run Tecnomatix_<TecnomatixVersion>_<ControllerName>_NNBIT_vVV_MM_DD_YYYY.exe.

The default installation point is C:\Program Files\Tecnomatix.

If you have any issues with the installation or support of these fixes,

please contact your local GTAC support group.

Sincerely,

Siemens Digital Industries Software

KB Article ID# PL8751750

Contents

SummaryDetails

Associated Components