Cannot specify STEP 242 Base Parts in NX2027

2024-02-12T21:04:45Z

Summary


Details

User are unable to reference null files for STEP242 translators in NX2007 series.

Platforms
  • na windows-1064
Release Versions
  • NX V2023
Solution

The capability to reference the null files for STEP242 was first made available in NX2206. so this cannot be done in NX2007 series.

In NX2206, the variables were inadvertently omitted, so the user can manually add the following statements to the step242ug.def file in the ../TRANSLATORS/step242 folder

BASE_PART_MM =<your UGII_BASE_DIR here>/TRANSLATORS/step242/step242null_mm.prt

BASE_PART_IN = <your UGII_BASE_DIR here>/TRANSLATORS/step242/step242null_in.prt

This will allow the user to customize the STEP242 template files to their specifications.

Notes

In NX2212 and later releases, we added the following additional STEP242 base parts which are referenced in the def files:

BASE_PART_MICRON = step242null_micron.prt

BASE_PART_MM = step242null_mm.prt

BASE_PART_METER = step242null_meter.prt

BASE_PART_IN = step242null_in.prt

KB Article ID# PL8751415

Contents

SummaryDetails

Associated Components