We have integrated Teamcenter with Solid Edge & configured Standard Parts to work with Teamcenter. After adding parts to the database, we are getting errors when placing them in assembly or generating them from the Database Administrator.
This issue is because of the mandatory custom property which does not have any default initial value set. To fix the issue set the default initial value to the mandatory custom property.