Rerouting connections fail in some environments

2023-09-26T06:17:16Z

Summary


Details

Why does rerouting connections fail in some environments?

Solution

If the assembly load options for reference sets have the below settings.

 Reference Sets    : Use Model, As Saved, Entire Part, Empty

                          

Auto route may not work.

The above setting forces the components to load "Model" reference set

Model reference sets do not have routing ports.

As ports are essential for "Auto route", It fails.

It is necessary to load a reference set that contains ports (or Entire part reference set)  for auto route to work

KB Article ID# PL8750664

Contents

SummaryDetails

Associated Components