Explain the details of columns used in sheetmetal material table.

2023-09-26T06:03:35Z

Summary


Details

Please explain the details of below columns used in sheetmetal material table

 i.e. "%UGII_BASE_DIR%\UGII\materials\sheet_metal_material_table.txt"

・Bare_or_Clad

・Cat

・THICKNESS

・BEND_RADIUS

・NEUTRAL_FACTOR

・RELIEF_DEPTH

・RELIEF_WIDTH

・JOGGLE_RADIUS

・JOGGLE_LENGTH

・Lightening_Cutout

Solution

・Bare_or_Clad

Can be used to define a material as a Bare/Clad material. This will enable the user to filter a specific material easily

For e.g. Clad Aluminimum, Bare Aluminium

・Cat

Can be used to define a category of material like metal/alloy etc.. This will enable the user to filter a specific material easily

・THICKNESS

Can be used to define the thickness of the material.

i.e. When a specific material is selected for a sheetmetal from sheetmetal preferences, the predefined thickness in the table will be applied.

・BEND_RADIUS

Can be used to define Bend radius of a sheetmetal.

For. e.g. applicable in Flange command

・NEUTRAL_FACTOR

Can be used to define Neutral factor of a sheetmetal.

For. e.g. applicable in Flange command

・RELIEF_DEPTH

Can be used to define relief depth of sheetmetal

For. e.g. applicable in Flange command

・RELIEF_WIDTH

Can be used to define relief width of a sheetmetal.

For. e.g. applicable in Flange command

・JOGGLE_RADIUS

Can be used to define joggle radius s of a sheetmetal.

For. e.g. applicable in Joggle command

・JOGGLE_LENGTH

Can be used to define joggle length  of a sheetmetal.

For. e.g. applicable in Joggle command

KB Article ID# PL8750659

Contents

SummaryDetails

Associated Components