How to create a Threaded Hole of custom dimeter and thread pitch

2023-11-07T08:19:21Z

Summary


Details

User need custom thread pitch in thread feature which can be editable as per their need

Solution

User can create a Threaded Hole of custom dimeter and thread pitch by editing the xlsx files in '~:\Program Files\Siemens\Solid Edge 2023\Preferences\Holes' folder.

For example:

You are using 'ISO Metric.xlsx' for creating a Threaded Hole feature in my part where you need to create a custom simple threaded hole of diameter M23 x 0.85mm Pitch (which is a non standard hole parameters).

Steps:

- In your 'ISO Metric.xlsx' in '~:\Program Files\Siemens\Solid Edge 2023\Preferences\Holes' folder; you should add an entry for it.


- Save and close the xlsx file

- Star a new part file and create block protrusion.

- In Solids > Holes command > Select Hole Options

- Select Threaded Hole type then select the custom hole of M23 x 0.85


- This is how you can create a non standard threaded hole with custom Pitch.


The thread Pitch can be edited in the xlsx file.

Notes

10791794

KB Article ID# PL8750552

Contents

SummaryDetails

Associated Components