During Flat pattern export from NX to Teamcenter, the dataset name is appearing as "Flat pattern export".
How to export flat pattern dataset to Teamcenter, with dataset name as ItemID_RevID ?
SolutionCurrently controlling the flat pattern dataset naming is supported for the custom datasets only.
With the default flat pattern dataset type, dataset naming will be created as "Flat pattern Export" only.
You need to define a custom dataset type for a DXF file to control the output naming of the flat pattern dataset.
Please refer to the below documentation for the required procedure to accomplish this.
https://docs.sw.siemens.com/en-US/doc/209349590/PL20200605195244930.nx_sheet_metal/xid1674612
https://docs.sw.siemens.com/en-US/doc/209349590/PL20200605195244930.nx_sheet_metal/xid1875497
https://docs.sw.siemens.com/en-US/doc/209349590/PL20200605195244930.nx_sheet_metal/xid1875501