Setting Machine Collision Check with an Inactive Spindle

2023-09-19T09:11:06Z

Summary


Details

There may be a requirement in manufacturing processes where spindle rotation is deactivated. When the spindle is inactive, the standard collision checks, Tool/IPW and Tool/Part are not used. This could be a problem for users and fail in identifying collisions within the simulation, potentially resulting in on-machine incidents. 

In the example provided a simple milling toolpath is shown which initially has the spindle rotating and material is correctly removed in the simulation. 

Figure 1 - Spindle rotating with material removed.

The 'Spindle Off' user defined event (UDE) is added which will add an M5 code to the NC output, deactivating the spindle rotation.  

Figure 2 - Spindle Off UDE.

Running the simulation again shows that the spindle rotation is inactive and the material is not removed, however, this would generate a clear collision on the machine. Tool/IPW and Tool/Part collision checks are enabled but as the spindle is inactive these checks are not used.

Figure 3 - Spindle inactive.

Figure 4 - Tool/IPW & Tool/Part Collision Checks enabled. 

Solution

In order to ensure collisions are checked in this scenario, machine collisions and collision pairs must be specified. 

To achieve this, open the Simulation Settings dialog and enable 'Check for Collision' under the Machine Collisions section. 

Figure 5 - Simulation Settings. 

It is then possible to 'Specify Collision Pairs. In this dialog, set the tool and workpiece as a pair. 

Figure 6 - Specify Collision Pairs. 

Once defined and running the simulation again shows that the collisions are identified and a Collision Violation warning appears. Now the user is aware of the potential risk associated with this operation. 

Figure 7 - Collision Violation. 

Notes

KB Article ID# PL8749068

Contents

SummaryDetails

Associated Components