Double weight for Sheet metal part in ANT Mass row.

2023-09-14T05:16:46Z

Summary


Details

In some cases it is necessary to omit certain weights from the calculation so as not to distort the total weight.

Solution

Example: 


1.Open assembly.

2.[Unpack All] if Pack component in Assembly Pattern.

3.Select Flat pattern reference component.

4.Menu>Analysis>Advanced Mass Properties>Show Mass Properties Panels.

5.Add Asserted Value as zero [0].

6.set Source as Asserted and Update Mass Properties.

7. Note: In ANT the Mass of the [FLAT PATTERN] displayed as [zero] so zero mass considered in the total Mass calculation.


Which is helps us to maintain single part/component Mass.     

KB Article ID# PL8744111

Contents

SummaryDetails

Associated Components