In a Teamcenter managed environment the customer wants to display the Project ID on a Solid Edge draft. According to the SEEC Administrator's guide we do not support attribute mapping to the Project ID.
So. how can we add the Teamcenter Project ID to a Solid Edge draft?
SolutionAccording to the documentation mapping to Project ID is not supported. However, this limitation is only for writing a project ID to Teamcenter. In this case, to display the Project ID on a draft, a mapping with the qualifier /master=iman is allowed.
Therefore, you can create a mapping for the Solid Edge draft only
and add a calllout on the draft to display the Project ID value.