"VCHIO" addition to MCF (simulation generates parse error while testing)

2023-09-25T11:24:41Z

Summary


Details


Solution

OKUMA has different controller modes. The supported variable names depend on this mode. The mode is changed with the CSE command SetControllerMode. Calling SetControllerMode("millinglathe") should establish the mode that supports variables starting with "VC".

Our default (used in OKUMA.CCF) is SetControllerMode("milling"). You need to change this if this machine requires a different mode.

KB Article ID# PL8739518

Contents

SummaryDetails

Associated Components