Solid Edge Solid Edge 2023 Update 0008 Announcement

2023-09-08T19:22:50Z
SE_BETA SE_TSS DOC_MANAGEMENT FLOEFD 3D-SKETCH SIMULATION Teamcenter Share TECH_PUB ASSEMBLY APPLICATION PART/SHEETMETAL TRANSLATORS DRAFT SETUP Solid Edge Marketing

Summary


Details

September 8, 2023

Dear Solid Edge Customer:

Solid Edge 2023 Update 0008 is now available for download.

We appreciate your continued business and participation in the software support process - - your reporting helps us make Solid Edge more productive for how you do business.

Sincerely,

The Solid Edge Team

============

Release Notes:

Solid Edge 2023 Update 0008

Version: 2210.0008.004 x64

Download Solid Edge 2023 (v2210) Updates

Note: if the direct download URL doesn't resolve in your browser, please navigate from the top-level Support Center.

===============

Email Notification:

===============

To receive direct email notifications for Solid Edge Updates, navigate to your Support Center Profile (https://account.sw.siemens.com/profile, scroll to Newsletter Subscriptions, and check the box for Software Field Bulletin

==========================================

This Solid Edge Update resolves the following PRs:

==========================================

===Assembly===

PR 10642706: Cannot select sketch in "assembly feature pattern" -> "sketch step"

PR 10719428: Dimension error assembly feature

PR 10721479: Mirror part vanishes after a suppress

PR 10739339: A drawing view is not correctly showing multibody parts that are overridden

PR 10740411: Pattern parts of pattern doesn't work for adjustable parts

PR 10789880: Applying Cutting Plane to assembly with zone closes Solid Edge

PR 10796502: DeleteInvalidSites.exe macro deleting valid links with no prompt

PR 10797923: SE crashes when showing the live sections of the specific assembly

PR 10482156: Cannot use curve segment

PR 273524: Modifications to a Part used in assembly feature is not reflected in the assembly

PR 333471: an abort using the Replace Part command and Component Finder

PR 334077: Component Search results showing components in simplified subassemblies

PR 231670: Problem locating items in Pathfinder after you scroll with the mouse wheel

===Draft===

PR 10789256: Crash during the drawing process

PR 322377: Some profile dimensions on an assembly cutout are not retrieved

===Part/Profile/Sheetmetal===

PR 10677283: crash after creating a 3D sketch

PR 10721274: Unable to generate physical thread

PR 10770739: Behavior change between SE 2022 and SE 2023 Move faces command

PR 10798254: Crash after creating a dimple feature

PR 10787730: API ExportDesignCostToCSV produces unreadable with “dot” decimal separator

===SEEC===

PR 10752620: Synchronizing the structure when opening an assembly.

===Translators===

PR 10441588: IFC Import generates overlapping, wrong size, wrong shape, and missing parts

PR 10716702: File name and instance name required as per model name

PR 10757943: 2nd run of the SW Data Migration is interrupted by "Save As" requests

PR 8683887: Error while Migrating Creo Element data

===Tech Pub===

PR 10786471: 3D Publishing crashes during export to PDF

=== PCB Collaborator===

PR 10795246: PCB Collaborator takes a long time to process

KB Article ID# PL8739487

Contents

SummaryDetails

Associated Components

SE_BETA