Solid Edge Open in Solid Edge button is not visible in Content tab of Active workspace

2024-08-28T12:38:48Z
DOC_MANAGEMENT

Summary


Details

"Open in Solid Edge" is not available in the content view for Solid Edge assemblies. It is available for other file types, and for assemblies in other views.

Platforms
  • all n/a-n/a
Release Versions
  • Solid Edge V222.0
Solution

The Teamcenter preference "AWC_AlternateSelectionCommandsList" needs to have the value "Awp0OpenInSEEC". Add that value to the preference and close and reopen Active Workspace on the clients to resolve the issue. This should work for standalone Active Workspace and hosted Active Workspace.

Notes

KB Article ID# PL8738225

Contents

SummaryDetails

Associated Components

DOC_MANAGEMENT: SEEC