Recommended versions of Windows 11 for SE2023

2023-08-29T14:55:26Z

Summary


Details

What are the current recommended versions of Windows 11 for Solid Edge 2023?

Solution

All versions of Windows 11 Professional and higher editions that are currently in the active servicing timeline provided by Microsoft (https://learn.microsoft.com/en-us/windows/release-health/windows11-release-information) during the active maintenance period of Solid Edge 2023 (https://support.sw.siemens.com/en-US/knowledge-base/PL8000986) are supported

Our recommendation has always been that customers should delay taking Windows 11 Feature Updates (new versions/operating systems) for as long as possible (https://support.sw.siemens.com/knowledge-base/PL8008188). This is because we believe that maturer Windows 11 versions provide for more overall stability than newer recently released Windows 11 versions.

As the maturest Windows 11 version approaches end of servicing with Microsoft we would then recommend that customers begin migrating over to the next maturest Windows 11 version that is actively supported by Microsoft.

As such, at this time, we recommend that customers should be using Windows 11 version 21H2 as it is the most mature actively supported version of Windows 11. As 21H2 approaches end of servicing with Microsoft we would then recommend customers begin migrating over to the next maturest supported version of Windows 11 which is currently version 22H2.

KB Article ID# PL8737513

Contents

SummaryDetails

Associated Components