Callouts in NX are not synchronized to Find Nos. in Structure Manager

2023-08-28T13:05:48Z

Summary


Details

Changing a callout number in NX does not sync to the same component in Structure Manager.

Solution

To synch Callouts to Find Numbers in Teamcenter, you need to change the "Object Selection" to "Apply to Component Instance" when editing the attribute in NX.

1. Right click the component -> Properties -> Attributes.

2. Under the Apply To dropdown in the Context section, select Instance.

3. Edit the CALLOUT attribute value -> OK.

4. The Find No. in Teamcenter Structure Manager will update.

KB Article ID# PL8736979

Contents

SummaryDetails

Associated Components